AXIS#.VL.KP
Description
AXIS#.VL.KP sets the proportional gain of the velocity loop.
The idealized velocity loop bandwidth
In computer networking, bandwidth often refers to a data rate measured in bits/s, for example, network throughput. The reason for the connection of data rate with the term bandwidth is that the limit to the data rate of a physical communication link is related to its bandwidth in hertz in Hz is:
Rotary motor:
Bandwidth
In computer networking, bandwidth often refers to a data rate measured in bits/s, for example, network throughput. The reason for the connection of data rate with the term bandwidth is that the limit to the data rate of a physical communication link is related to its bandwidth in hertz (Hz) = AXIS#.VL.KP *Kt/ (2π *Jm)
Where:
Kt= motor torque
Torque is the tendency of a force to rotate an object about an axis. Just as a force is a push or a pull, a torque can be thought of as a twist constant, in units of Nm/Arms
Jm = motor inertia, in units of kg*m²
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
A/(rad/sec) |
|
Range |
0 to 2,147,483.008 |
|
Default Value |
0 |
|
Data Type |
Float |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
| Fieldbus |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO |
|---|---|---|---|---|---|---|---|---|
| EtherCAT |
AXIS1.VL.KP | 0x5011 | 0x1 | DINT | 1000:1 | - | RW | False |
| AXIS2.VL.KP | 0x5111 | 0x1 | DINT | 1000:1 | - | RW | False |